Zoek op trefwoord, order- of productcode of serienummer, bv. “CM442” of “Technische informatie”
Voer tenminste 2 karakters in om het zoeken te starten.
  • Geschiedenis

Endress+Hauser development team earns the AMA Innovation Award

iTHERM TrustSens recognized as an exceptional innovation in the field of sensors and instrumentation

Publicatiedatum: 26.06.2018

With its innovation, the development team from Endress+Hauser Wetzer, the center of competence for temperature measurement technology headquartered in Nesselwang, Germany, prevailed against 35 German and international competitors to win the award. The iTHERM TrustSens thermometer was designed especially for hygienic and aseptic applications in the food & beverage and life sciences industries.

The instrument features automated and fully traceable inline self-calibration, eliminating the risk of non-conformities and leading to superior product safety and process efficiency. In addition, the integrated Heartbeat Technology enables continuous self-diagnosis and verification without interruption of the process.

The AMA Innovation Award, which is given to innovative research and development teams by the AMA Association for Sensors and Measurement, is considered one of the industry’s most coveted awards. The awards ceremony was held on 26 June 2018 during the Sensor+Test trade fair in Nuremberg, Germany. The Promass Q Coriolis-based flowmeter from Endress+Hauser was also nominated.

Further information about the award-winning product, plus an interview with the development team, is available in the downloads section in the right-hand column.

Lees over vergelijkbare onderwerpen

Downloads

    DE_Hintergrundtext_Interview_iTHERM TrustSens.zip

    EH_Media Release_AMA Award_26-06-2018.zip

Perslijst

Ontvang de volgende persberichten en het volgende nieuws rechtstreeks in uw mailbox. Blijf op de hoogte door u te abonneren op de perslijst van Endress+Hauser.

Endress+Hauser press list

Endress+Hauser regularly sends out press releases on current topics and company information to media professionals.

Select the topics you are interested in: *
Select the industries you are interested in:

Do you want to receive invitations to Endress+Hauser (digital or live) press events? 

Personal data

Fields marked with * have to be filled out. You will receive an email with a confirmation of your subscription and the related internet link. Your data will only be used for personalizing your newsletters and will not be passed on to any third party. The information enlisted is voluntarily. For statistical reasons we will perform anonymous link tracking.

Contact