Zoek op trefwoord, order- of productcode of serienummer, bv. “CM442” of “Technische informatie”
Voer tenminste 2 karakters in om het zoeken te starten.
  • Geschiedenis

Endress+Hauser establishes internet security standards

IETF recommends the SmartBlue CPace protocol for password-protected access to instruments

The cryptography working group within the IETF standards organization (Internet Engineering Task Force) has chosen the Endress+Hauser-developed CPace protocol as a recommended method for use in internet standards. After undergoing extensive security analyses, the CPace protocol emerged as the winner in a competition among submissions from developers at several well-known companies.

Secure access to field instruments is of the highest priority for operators across all branches of the process industry. Modern plants contain hundreds or thousands of measurement and control instruments that must be accessed remotely with growing frequency. These field instruments also have to be installed, monitored or serviced on a regular basis. Secure password-based user authentication plays a special role today, especially when devices with digital interfaces are involved.

Security with user-friendly password lengths

In order to utilize Bluetooth communications technology in industrial environments, security experts at Endress+Hauser identified a need for additional protection. The result was the development of a solution called CPace, which belongs to the class of PAKE (password-authenticated key exchange) methods. Among other things, PAKE technology is used with the German electronic ID cards as a means of largely decoupling the cryptographic security level from the length of the password.

The advantage of this method is that the processing power of even the smallest of field instruments is sufficient to provide devices, and thus the industrial systems, with the best level of protection against cyberattacks. At the same time CPace enjoys a high degree of acceptance among users given that the desired level of security can be achieved without relying on long passwords.

“We had to look internally to find a solution for establishing secure connections to the instruments. Previously available methods were out of the question because they provide an inadequate level of security given that field instruments have limited processing power and storage capacity. Password verification would have meant a login delay of two minutes or more,” explains Dr Björn Haase, head of the project at Endress+Hauser.

CPace makes life difficult for hackers

The security of the PAKE-based solution with Bluetooth technology from Endress+Hauser was previously verified in 2016 as part of an analysis by the Fraunhofer Institute for Applied and Integrated Security (AISEC). The institute classified the protection level of the Endress+Hauser security layer, the core component of which is recommended for use in internet environments, as “high”.

Modern plants contain hundreds or thousands of measurement and control instruments. ©Endress+Hauser

Modern plants contain hundreds or thousands of measurement and control instruments. Secure password-based access to the instruments is thus becoming increasingly important.

With the CPace protocol, Endress+Hauser ensures secure access to field instruments. ©Endress+Hauser

With the CPace protocol, Endress+Hauser ensures secure access to field instruments.

Dr. Björn Haase, Senior Expert Electronics at Endress+Hauser Liquid Analysis. ©Endress+Hauser

Dr. Björn Haase, Senior Expert Electronics at Endress+Hauser Liquid Analysis.

Contact